lpuart_9bit_transfer
Overview
The lpuart_9bit_transfer example shows how to use lpuart driver in 9-bit mode.
In this example, one lpuart instance is used with 9bit mode. Its TX and RX pins are connected together. The data with 9bit can be received by itself. The each data in TX and RX data register will be 16-bit data.