mcan_loopback

Overview

The mcan_loopback example shows how to use the loopback test mode to debug your CAN Bus design:

To demonstrate this example, only one board is needed. The example will config Tx Buffer to send and Rx Fifo to receive. After that, the example will send a CAN Message throuth internal loopback interconnect and print out the Message payload to the terminal.

Supported Boards