mcx_opamp_basic
Overview
The OPAMP basic example demonstrates how to use the OPAMP driver. In this example, the OPAMP works in the internal gain mode, connect the positive terminal of the OPAMP to the external input source. The OPAMP output is 2X of the external input voltage. When the input voltage changes, the OPAMP output changes accordingly.