queued_spi_edma_b2b_transfer_slave
Overview
The queued_spi_edma_b2b_transfer example shows how to use QUEUEDSPI driver in edma way:
In this example, we need two boards, one board is used as QUEUEDSPI master and another board is used as QUEUEDSPI slave. The file ‘queued_spi_edma_b2b_transfer_slave.c’ includes the DSPI slave code.
QUEUEDSPI master sends/receives data to/from QUEUEDSPI slave in edma way. (QUEUEDSPI Slave uses edma way to receive/send the data)