csi_mipi_rgb
Overview
This project shows how to use the CSI with MIPI_CSI. In this example, the camera device output pixel format is RGB565, the MIPI_CSI converts it to RGB888 internally and sends to CSI. In other words, the CSI input data bus width is 24-bit. The CSI saves the frame as 32-bit format XRGB8888. PXP is used to convert the XRGB8888 to RGB565 and shown in the LCD panel.