csi_mipi_yuv
Overview
This project shows how to use the CSI with MIPI_CSI. In this example, the camera device output pixel format is YUYV, the MIPI_CSI converts it to YUV internally and sends to CSI. In other words, the CSI input data bus width is 24-bit. The CSI saves the frame as 32-bit format XYUV8888. PXP is used to convert the XYUV to RGB565 and show in the LCD panel.