flexcan_efifo_edma_transfer

Overview

The flexcan_efifo_edma_transfer example shows how to use the EDMA version transactional driver to receive CAN FD Message from Enhanced Rx FIFO:

In this example, when setting ENABLE_LOOPBACK macro, only one board is needed. The example will config one FlexCAN Message Buffer to Tx Message Buffer and setup Enhanced Rx FIFO. After that, the example will send 4 CAN FD Messages from Tx Message Buffer to Enhanced Rx FIFO through internal loopback interconnect and read them out using EDMA version FlexCAN transactional driver. The sent and received message will be print out to terminal.

2 boards are required to be connected through CAN bus if ENABLE_LOOPBACK is not defined. Endpoint A(board A) send a CAN Message to Endpoint B(board B) when user press space key in terminal. Endpoint B receives the message by Enhanced Rx FIFO and reads them out using EDMA version FlexCAN transactional driver. The sent and received message will be print out to terminal.

Supported Boards