MCUXpresso SDK Documentation

lpc_bod

lpc_bod#

Overview#

The bod example shows how to use LPC BOD(Brown-out detector) in the simplest way. To run this example, user should remove the jumper for the power source selector, and connect the adjustable input voltage to the MCU’s Vin pin. If the input voltage of the Vin pin is lower than the threshold voltage, the BOD interrupt will be asserted.

Supported Boards#