MCUXpresso SDK Documentation

s3mu#

Overview#

The S3MU Example project is a demonstration program that uses the MCUX SDK software to show basic communication with EdgeLock Enclave (ELE) and usage of its services with direct use of S3MU driver.

Running the demo#

Example output on terminal:

TODO

Supported Boards#

MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

S3MU Driver Example:

****************** Ping EdgeLock **************************
S3MU Driver Ping command sucessfully.

End of Example with SUCCESS!!
FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

S3MU Driver Example:

****************** Ping EdgeLock **************************
S3MU Driver Ping command sucessfully.

End of Example with SUCCESS!!