ostimer_example

Overview

The OSTIMER project is a simple demonstration program of the SDK OSTIMER driver. It sets the OSTIMER as the wakeup source from deep-sleep mode. Board will enter power deep sleep mode, and then wakeup by OS timer after about 5 seconds. After wakeup from deep-sleep mode, OS timer will set match value to trigger the interrupt while the timer count tick reach the match value about every 2 seconds.

Supported Boards