MCUXpresso SDK Documentation

gdet

gdet#

Overview#

Running the demo#

When the demo runs successfully, the terminal displays similar information like the following:


GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

## Supported Boards
- [FRDM-MCXN947](../../_boards/frdmmcxn947/driver_examples/gdet/example_board_readme.md)
- [MCX-N5XX-EVK](../../_boards/mcxn5xxevk/driver_examples/gdet/example_board_readme.md)
- [MCX-N9XX-EVK](../../_boards/mcxn9xxevk/driver_examples/gdet/example_board_readme.md)
- [MIMXRT700-EVK](../../_boards/mimxrt700evk/driver_examples/gdet/example_board_readme.md)
- [FRDM-IMXRT700](../../_boards/frdmimxrt700/driver_examples/gdet/example_board_readme.md)
- [FRDM-MCXA577](../../_boards/frdmmcxa557/driver_examples/gdet/example_board_readme.md)
- [FRDM-KW43](../../_boards/frdmkw43/driver_examples/gdet/example_board_readme.md)
- [FRDM-MCXW70](../../_boards/frdmmcxw70/driver_examples/gdet/example_board_readme.md)
- [FRDM-MCXA287](../../_boards/frdmmcxa287/driver_examples/gdet/example_board_readme.md)