lptmr#
Overview#
The LPTMR project is a simple demonstration program of the SDK LPTMR driver. It sets up the LPTMR hardware block to trigger a periodic interrupt after every 1 second. When the LPTMR interrupt is triggered a message is printed on the UART terminal and an LED is toggled on the board.
Supported Boards#
EVK9-MIMX8ULP
Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
IMX952LPD5EVK-19
Hardware requirements
Micro USB cable
IMX952-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
EVK-MCIMX7ULP
Hardware requirements
Micro USB cable
MCIMX7ULP-EVK board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW1 to power on the board.
Connect a micro USB cable between the host PC and the J6 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
EVK-MIMX8ULP
Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
MIMXRT1180-EVK
Hardware requirements
Micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
FRDM-K22F
Hardware requirements
Mini/micro USB cable
FRDM-K22F board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
And you will find the LED RED is taking turns to shine.
FRDM-K32L2A4S
Hardware requirements
Mini/micro USB cable
FRDM-K32L2A4S board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-K32L2B
Hardware requirements
Mini/micro USB cable
FRDM-K32L2B board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-K32L3A6
Hardware requirements
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: LPTMR hardware block of FRDM-KE15Z board will trigger a periodic interrupt after every 0.5 second instead of 1 second as other boards. When the example runs successfully, the following message is displayed in the terminal and you will find the LED RED is taking turns to shine.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
FRDM-KE16Z
Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: LPTMR hardware block of FRDM-KE16Z board will trigger a periodic interrupt after every 0.5 second instead of 1 second as other boards. When the example runs successfully, the following message is displayed in the terminal and you will find the LED RED is taking turns to shine.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
FRDM-KE17Z
Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: LPTMR hardware block of FRDM-KE17Z board will trigger a periodic interrupt after every 0.5 second instead of 1 second as other boards. When the example runs successfully, the following message is displayed in the terminal and you will find the LED RED is taking turns to shine.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
FRDM-KE17Z512
Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: LPTMR hardware block of FRDM-KE17Z board will trigger a periodic interrupt after every 0.5 second instead of 1 second as other boards. When the example runs successfully, the following message is displayed in the terminal and you will find the LED RED is taking turns to shine.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
FRDM-MCXA153
Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA156
Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA346
Hardware requirements
Type-C USB cable
FRDM-MCXA346 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXC041
Hardware requirements
Type-C USB cable
FRDM-MCXC041 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-MCXC242
Hardware requirements
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-MCXC444
Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-MCXE247
Hardware requirements
USB-C cable
FRDM-MCXE247 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: LPTMR hardware block of FRDM-MCXE247 board will trigger a periodic interrupt after every 0.5 second instead of 1 second as other boards. When the example runs successfully, the following message is displayed in the terminal and you will find the LED RED is taking turns to shine.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
FRDM-MCXN236
Hardware requirements
Type-C USB cable
FRDM-MCXN236 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the type-c and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXW71
Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
MCX-W71-EVK
Hardware requirements
Type-C USB cable
MCX-W71-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
IMX95LPD5EVK-19
Hardware requirements
Micro USB cable
IMX95LPD5-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
FRDM-IMX95
Hardware requirements
Micro USB cable
FRDM-IMX95 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
FRDM-IMX952
Hardware requirements
Micro USB cable
IMX952-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
FRDM-IMX937
Hardware requirements
Micro USB cable
FRDM-IMX937 board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
KW45B41Z-EVK
Hardware requirements
Mini/micro USB cable
KW45B41Z-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
KW47-EVK
Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
MCIMX93AUTO-EVK
Hardware requirements
USB Type-C cable
MCIMX93AUTO-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.
Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
MCIMX93-EVK
Hardware requirements
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
MCIMX93W-EVK
Hardware requirements
USB Type-C cable
MCIMX93W-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
MCIMX93-QSB
Hardware requirements
USB Type-C cable
MCIMX93-QSB board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
IMX943-EVK
Hardware requirements
Micro USB cable
IMX943-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.
Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
MCX-W72-EVK
Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
TWR-KM34Z50MV3
Hardware requirements
Mini USB cable
TWR-KM34Z50MV3 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
TWR-KM34Z75M
Hardware requirements
Mini USB cable
TWR-KM34Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
TWR-KM35Z75M
Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the LED RED is taking turns to shine.
FRDM-MCXL255
Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
Make sure you have solder bridges SJ1 and SJ2 set to
2-1 for the main core (cm33)
2-3 for AON core (cm0+)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA174
Hardware requirements
Type-C USB cable
FRDM-MCXA174 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA344
Hardware requirements
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
KW47-LOC
Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
MCXW72-LOC
Hardware requirements
Type-C USB cable
MCXW72-LOC Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-IMXRT1186
Hardware requirements
Micro USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
These instructions are displayed/shown on the terminal window:
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
....................
....................
~~~~~~~~~~~~~~~~~~~~~~~
FRDM-MCXA266
Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA366
Hardware requirements
Type-C USB cable
FRDM-MCXA366 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXW72
Hardware requirements
Type-C USB cable
FRDM-MCXW72 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXC162
Hardware requirements
Type-C USB cable
FRDM-MCXC162 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXW70
Hardware requirements
Type-C USB cable
FRDM-MCXW70 Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J28.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6
FRDM-MCXA287
Hardware requirements
Type-C USB cable
FRDM-MCXA287 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the USB Type-C cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Low Power Timer Example
LPTMR interrupt No.1
LPTMR interrupt No.2
LPTMR interrupt No.3
LPTMR interrupt No.4
LPTMR interrupt No.5
LPTMR interrupt No.6