MCUXpresso SDK Documentation

rtc_1

rtc_1#

Overview#

The RTC project is a simple demonstration program of the SDK RTC driver. It sets up the RTC hardware block to trigger an alarm after a user specified time period. The test will set the current date and time to a predefined value. The alarm will be set with reference to this predefined date and time.

Supported Boards#

FRDM-KE02Z40M
Hardware requirements
  • Mini/micro USB cable

  • FRDM-KE02Z40M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

RTC example: set up time to wake up an alarm.
Current datetime: 2014-12-25 19:00:00
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19:01:11

Alarm occurs !!!! Current datetime: 2014-12-25 19:01:11
Please input the number of second to wait for alarm
The second must be positive value
...............................................
...............................................