flashiap#
Overview#
The FLASIAP project is a simple demonstration program of the SDK FLASIAP driver. It erases and programs a portion of on-chip flash memory. A message a printed on the UART terminal as various operations on flash memory are performed.
Supported Boards#
LPCXpresso51U68
Hardware requirements
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
FLASHIAP example
Writing flash sector 1
Erasing flash sector 1
Erasing page 1 in flash sector 1
End of FLASHIAP Example
LPCXpresso54628
Hardware requirements
Micro USB cable
LPCXpresso54628 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The following lines are printed to the serial terminal when the demo program is executed.
FLASHIAP example
Writing flash sector 1
Erasing flash sector 1
Erasing page 1 in flash sector 1
End of FLASHIAP Example