19 #include "clock_config.h"    21 #include "fsl_debug_console.h"    26 #include "Driver_I2C.h"    31 #include "issdk_hal.h"    32 #include "gpio_driver.h"    42 #define FF_MT_WT_DBCNT 0x18      43 #define FF_MT_THS_VALUE 0x08    117     PRINTF(
"\r\n ISSDK MMA865x sensor driver example for Freefall Detection. \r\n");
   124     if (ARM_DRIVER_OK != status)
   126         PRINTF(
"\r\n I2C Initialization Failed\r\n");
   131     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   132     if (ARM_DRIVER_OK != status)
   134         PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
   139     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   140     if (ARM_DRIVER_OK != status)
   142         PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
   151         PRINTF(
"\r\n Sensor Initialization Failed\r\n");
   154     PRINTF(
"\r\n Successfully Initialized Sensor\r\n");
   163         PRINTF(
"\r\n MMA865x Sensor Configuration Failed, Err = %d \r\n", status);
   166     PRINTF(
"\r\n Successfully Applied MMA865x Sensor Configuration for Freefall Detection\r\n");
   167     PRINTF(
"\r\n MMA865x is now active and detecting freefall... \r\n");
   183         PRINTF(
"\r\n Freefall detected !!!\r\n");
 #define MMA865x_CTRL_REG1_DR_MASK
#define MMA865x_FF_MT_CFG_YEFE_MASK
#define MMA865x_CTRL_REG1_DR_200HZ
This structure defines the Write command List. 
This defines the sensor specific information. 
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_INT1
#define MMA865x_XYZ_DATA_CFG_FS_MASK
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
#define MMA865x_FF_MT_CFG_XEFE_EN
Access structure of the GPIO Driver. 
const registerwritelist_t cMma865xConfigFreeFall[]
Register settings for freefall detection. 
#define MMA865x_FF_MT_THS_THS_MASK
#define __END_WRITE_DATA__
#define MMA865x_CTRL_REG3_IPOL_MASK
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
const registerreadlist_t cMma865xFreeFallEvent[]
Address of Freefall Status Register. 
#define MMA865x_FF_MT_THS_DBCNTM_INC_CLR
#define MMA865x_CTRL_REG3_IPOL_ACTIVE_HIGH
#define I2C_S_SIGNAL_EVENT
#define MMA865x_FF_MT_CFG_ZEFE_EN
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_EN
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_MASK
int main(void)
This is the The main function implementation. 
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
GENERIC_DRIVER_GPIO * pGpioDriver
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
#define __END_READ_DATA__
void mma865x_isr_callback(void *pUserData)
This is the Sensor ISR implementation. 
The mma865x_drv.h file describes the MMA865x driver interface and structures. 
#define MMA865x_CTRL_REG1_ACTIVE_MASK
#define MMA865x_CTRL_REG1_ACTIVE_ACTIVATED
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_MASK
#define MMA865x_FF_MT_CFG_XEFE_MASK
volatile bool gMma865xIntFlag
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
#define MMA865x_XYZ_DATA_CFG_FS_2G
#define MMA865x_FF_MT_CFG_ZEFE_MASK
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
This structure defines the Read command List. 
#define I2C_S_DEVICE_INDEX
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
void BOARD_InitDebugConsole(void)
#define MMA8652_WHOAMI_VALUE
#define MMA865x_FF_MT_CFG_OAE_MASK
#define MMA865x_FF_MT_THS_DBCNTM_MASK
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features. 
#define MMA865x_FF_MT_CFG_OAE_FREEFALL
#define MMA865x_FF_MT_CFG_YEFE_EN