acmp_interrupt

Overview

The ACMP Interrupt project is a simple demonstration program that uses the SDK software. It compares the selected analog input with ACMP internal DAC output continuously and toggle the LED when the final comparison result changed. The purpose of this demo is to show how to use the ACMP driver in SDK software by interrupt way. The ACMP can be configured based on default configuration returned by the API ACMP_GetDefaultConfig(). The default configuration is: high speed is not enabled, invert output is not enabled, unfiltered output is not enabled, pin out is not enabled, offset level is level 0, hysteresis level is level 0.

Running the demo

Before example running, please connect the analog input voltage to stable external voltage generator to avoid floating voltage and adjust external voltage generator to be higher than reference DAC output (half of referene voltage) to make the initial comparison result to be 0.

When the demo runs successfully, following information can be seen on the terminal:

The example compares analog input to the reference DAC output(CMP positive port).
The LED will be turned ON/OFF when the analog input is LOWER/HIGHER than the DAC output.
Change the analog input voltage to see the LED status.
The analog input is LOWER than DAC output
The analog input is HIGHER than DAC output

Supported Boards