cadc_expansion_mux_aux_opamp#
Overview#
The CADC expansion mux aux OPAMP application demonstrates how to use an expansion of the ADC to implement voltage acquisition and change the gain of an operational amplifier. The OPAMP configuration has 4 different gains, namely X1, X2, X4, X8. Enter any key in the terminal to trigger ADC conversion to sample the OPAMP output, and switch the OPAMP gain at the same time. ADC Converter A and OPAMPA are used in pairs.
Supported Boards#
MC56F80000-EVK
Hardware requirements
Micro USB cable
MC56F80000-EVK board
Personal Computer
Board hardware common setting
Power setting:
Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2
Reset pin setting:
Connect J11 pin2 and pin3
Debugger setting:
Connect J13 pin 1-2, 3-4, 5-6, 7-8
Board settings
Remove jumper for J20, J15, J16. OPAMPA CH0 input signal J20-2(GPIOA1).The OPAMPA output signal (J1-10) is connected to the ANA4C (J1-12).
Prepare the Demo
Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.
Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with PnE U-MultiLink debug configuration.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
CADC expansion mux aux OPAMP example.
Press any key to trigger the conversion and toggle the OPAMP gain.
ADC Value: 3960
ADC Value: 7952
ADC Value: 15896
ADC Value: 31800
ADC Value: 3944
User can press any key to get converter data and toggle OPAMP gain.
The example initial OPAMP gain X1 , the OPAMP input voltage range is about 0-3.3v.
The first trigger ADC conversion, the OPAMP gain is switched to X1, the OPAMP input voltage range is about 0-3.3v.
The second trigger ADC conversion, the OPAMP gain is switched to X2, the OPAMP input voltage range is about 0-1.65v.
The third trigger ADC conversion, the OPAMP gain is switched to X4, the OPAMP input voltage range is about 0-0.82v.
The fourth trigger ADC conversion, the OPAMP gain is switched to X8, the OPAMP input voltage range is about 0-0.41v.