MCUXpresso SDK Documentation

i2c_read_fxls897x_accel_value_transfer

i2c_read_fxls897x_accel_value_transfer#

Overview#

The i2c_read_fxls897x_accel_value example shows how to use I2C driver to communicate with an i2c device:

  1. How to use the i2c driver to read a i2c device who_am_I register.

  2. How to use the i2c driver to write/read the device registers.

In this example, the values of three-axis accelerometer print to the serial terminal on PC through the virtual serial port on board.

Running the demo#

When the example runs successfully, you can see the similar information from the terminal as below.

I2C example – Read Accelerometer Value Found an FXLS8974 on board, the device address is 0x18. The accel values: x = -31 , y = -39 , z = 1301 x = -31 , y = -39 , z = 1301 x = -20 , y = -23 , z = 1305 x = -20 , y = -23 , z = 1305 x = -20 , y = -23 , z = 1305 x = -24 , y = -12 , z = 1275 x = -24 , y = -12 , z = 1275 x = -28 , y = -27 , z = 1290 x = -28 , y = -27 , z = 1290 x = -16 , y = -20 , z = 1316

End of I2C example.

Supported Boards#

FRDM-MCXC041
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXC041 board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXC242
Hardware requirements
  • USB-C cable

  • FRDM-MCXC242 board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

FRDM-MCXC444
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXC444 board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.