jpegdec_context_switch
Overview
The SD JPEG decoder example decodes a series of JPEG pictures stored on SD card then shows them one by one on panel. Two slots are used and each has one descriptor linked to itself. After slot 0 finishes slot 1 will be switch on in this round. After slot 1 finishes then the next round starts, slot 0 will be switched on again.