netc_psi_vsi_message

Overview

The Multicore NETC PSI-VSI demo application demonstrates how to set up projects for individual cores on a multicore system. In this demo, the primary core use NETC PSI to send/receive frames. It also releases the secondary core from the reset. The secondary core toggles an on-board LED indicating that the secondary core is running and uses NETC VSI to send/receive frames.

Supported Boards