pdb_delay_interrupt#
Overview#
The pdb_delay_interrupt example show how to use the PDB as a general programmable interrupt timer.
The PDB is triggered by software, and other external triggers are generated from PDB in this project, so that user can see just a general counter is working with interrupt.
Supported Boards#
FRDM-K22F
Hardware requirements
Mini/Micro USB cable
FRDM-K22F board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
PDB Delay Interrupt Example.
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 1
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 2
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 3
FRDM-KE15Z
Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
PDB Delay Interrupt Example.
Type any key into terminal to trigger the PDB counter ...
PDB Delay Interrupt Counter: 1
Type any key into terminal to trigger the PDB counter ...
PDB Delay Interrupt Counter: 2
Type any key into terminal to trigger the PDB counter ...
FRDM-KE16Z
Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
PDB Delay Interrupt Example.
Type any key into terminal to trigger the PDB counter ...
PDB Delay Interrupt Counter: 1
Type any key into terminal to trigger the PDB counter ...
PDB Delay Interrupt Counter: 2
Type any key into terminal to trigger the PDB counter ...
FRDM-MCXE247
Hardware requirements
USB-C cable
FRDM-MCXE247 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
PDB Delay Interrupt Example.
Type any key into terminal to trigger the PDB counter ...
PDB Delay Interrupt Counter: 1
Type any key into terminal to trigger the PDB counter ...
PDB Delay Interrupt Counter: 2
Type any key into terminal to trigger the PDB counter ...
TWR-KM34Z75M
Hardware requirements
Mini USB cable
TWR-KM34Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
PDB Delay Interrupt Example.
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 1
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 2
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 3
TWR-KM35Z75M
Hardware requirements
Micro USB cable
TWR-KM35Z75M board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
PDB Delay Interrupt Example.
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 1
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 2
Type any key into terminal to trigger the PDB counter … PDB Delay Interrupt Counter: 3