i2c_gpdma_b2b_transfer_master#
Overview#
The i2c_gpdma_b2b_transfer_master example shows how to use i2c driver as master to do board to board transfer with GPDMA:
In this example, one i2c instance as master and another i2c instance on the other board as slave. Master sends a piece of data to slave with desired buadrate’s, and receive a piece of data from slave. This example checks if the data received from slave is correct.
The desired baudrate’s are 100kHz,400kHz,1MHz, and 3.4MHz.