MCUXpresso SDK Documentation

ftm_pwm_twochannel

ftm_pwm_twochannel#

Overview#

The FTM pwm two channel Example project is a demonstration program that uses the KSDK software to generate a square pulse PWM(24kHZ) on 2 channel to control the LED brightness. It sets up the FTM hardware block to output two edge-aligned PWM signals. The PWM dutycycles are periodically updated.

  • FTM generates a PWM with the increasing and decreasing duty cycle.

  • LED brightness is increasing and then dimming. This is a continuous process. The user should probe the FTM output with a oscilloscope to see the PWM.

Supported Boards#