ftm_timer
Overview
The FTM project is a simple demonstration program of the SDK FTM driver to use FTM as a timer. It sets up the FTM hardware block to trigger an interrupt every 1 millisecond. When the FTM interrupt is triggered 1000 times, a message is printed on the UART terminal.