19 #include "clock_config.h" 21 #include "fsl_debug_console.h" 26 #include "Driver_I2C.h" 31 #include "issdk_hal.h" 32 #include "gpio_driver.h" 38 #define MT_FFMT_THS 0x07 39 #define MT_FFMT_COUNT 0x00 40 #define ASLP_COUNT 0x14 105 uint8_t eventStatus = 0;
108 uint8_t sleepflag = 1;
109 uint16_t eventDetectionCount = 0;
120 PRINTF(
"\r\n ISSDK MMA865x sensor example demonstration for Auto Wake Sleep feature.\r\n");
132 if (ARM_DRIVER_OK != status)
134 PRINTF(
"\r\n I2C Initialization Failed\r\n");
139 status = I2Cdrv->PowerControl(ARM_POWER_FULL);
140 if (ARM_DRIVER_OK != status)
142 PRINTF(
"\r\n I2C Power Mode setting Failed\r\n");
147 status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
148 if (ARM_DRIVER_OK != status)
150 PRINTF(
"\r\n I2C Control Mode setting Failed\r\n");
159 PRINTF(
"\r\n Sensor Initialization Failed\r\n");
162 PRINTF(
"\r\n Successfully Initialized Sensor\r\n");
171 PRINTF(
"\r\n MMA865x Sensor Configuration Failed, Err = %d \r\n", status);
174 PRINTF(
"\r\n Successfully Applied MMA865x Sensor Configuration for Auto-Wake-Sleep Mode\r\n\r\n");
175 PRINTF(
"\r\n MMA865x is now active and detecting sudden motion gesture of lifting up the board... \r\n\r\n");
183 if (ARM_DRIVER_OK != status)
196 eventDetectionCount++;
197 PRINTF(
"\r\n Sensor Detected Motion!!!\r\n");
198 PRINTF(
"\r\n Waking up MCU on motion detection event\r\n");
199 PRINTF(
"\r\n Total Motion Detection Events captured = %d\r\n", eventDetectionCount);
200 PRINTF(
"\r\n Will enter sleep mode automatically on expiry of ASLP Count = ~6sec\r\n");
201 PRINTF(
"\r\n ==================================================================\r\n\r\n");
211 if ((sleep == 1) || (sleepflag == 1))
213 PRINTF(
"\r\n No-Motion Detected - ASLP Counter = ~6sec Expired\r\n");
214 PRINTF(
"\r\n Going to Sleep Mode...\r\n");
215 PRINTF(
"\r\n Putting MCU in low power sleep\r\n");
216 PRINTF(
"\r\n ==================================================================\r\n\r\n");
void(* set_pin)(pinID_t aPinId)
#define MMA865x_CTRL_REG1_DR_MASK
#define MMA865x_FF_MT_CFG_YEFE_MASK
void mma865x_isr_callback(void *pUserData)
This is the Sensor ISR implementation.
#define MMA865x_CTRL_REG1_DR_800HZ
This structure defines the Write command List.
This defines the sensor specific information.
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_INT1
#define MMA865x_CTRL_REG3_WAKE_FF_MT_MASK
#define MMA865x_CTRL_REG1_ASLP_RATE_1_56HZ
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
#define MMA865x_FF_MT_CFG_XEFE_EN
int main(void)
This is the The main function implementation.
Access structure of the GPIO Driver.
const registerreadlist_t gMma8562ReadSysMode[]
Read register list for MMA8562 to read SysMode Register.
#define MMA865x_FF_MT_THS_THS_MASK
volatile bool gMma865xIntFlag
#define __END_WRITE_DATA__
#define MMA865x_CTRL_REG3_IPOL_MASK
void(* clr_pin)(pinID_t aPinId)
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
int32_t MMA865x_I2C_ReadData(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data.
#define MMA865x_CTRL_REG3_IPOL_ACTIVE_HIGH
#define I2C_S_SIGNAL_EVENT
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_EN
#define MMA865x_CTRL_REG4_INT_EN_FF_MT_MASK
#define MMA865x_CTRL_REG2_MODS_MASK
#define BOARD_BootClockRUN
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type.
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
int32_t MMA865x_I2C_Configure(mma865x_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor.
#define MMA865x_CTRL_REG1_ACTIVE_STANDBY
#define __END_READ_DATA__
The mma865x_drv.h file describes the MMA865x driver interface and structures.
#define MMA865x_CTRL_REG1_ACTIVE_MASK
#define MMA865x_CTRL_REG1_F_READ_MASK
#define MMA865x_SYSMOD_SYSMOD_WAKE
#define MMA865x_CTRL_REG5_INT_CFG_FF_MT_MASK
#define MMA865x_FF_MT_CFG_XEFE_MASK
const registerwritelist_t mma865x_autowake_motiondet_config[]
#define MMA865x_FF_MT_CFG_OAE_MOTION
#define MMA865x_CTRL_REG2_SMODS_MASK
#define MMA865x_CTRL_REG1_ASLP_RATE_MASK
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
This structure defines the Read command List.
gpioHandleKSDK_t GREEN_LED
#define I2C_S_DEVICE_INDEX
void MMA865x_I2C_SetIdleTask(mma865x_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task.
#define MMA865x_CTRL_REG2_SMODS_LP
#define MMA865x_CTRL_REG2_SLPE_MASK
void BOARD_InitDebugConsole(void)
#define MMA865x_CTRL_REG2_SLPE_EN
#define MMA8652_WHOAMI_VALUE
#define MMA865x_FF_MT_CFG_OAE_MASK
int32_t MMA865x_I2C_Initialize(mma865x_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor.
void BOARD_InitPins(void)
Configures pin routing and optionally pin electrical features.
#define MMA865x_CTRL_REG3_WAKE_FF_MT_EN
#define MMA865x_CTRL_REG2_MODS_LP
#define MMA865x_CTRL_REG1_F_READ_NORMAL
#define MMA865x_FF_MT_CFG_YEFE_EN