20 #include "clock_config.h"    25 #include "Driver_I2C.h"    26 #include "Driver_USART.h"    31 #include "issdk_hal.h"    32 #include "gpio_driver.h"    36 #include "auto_detection_service.h"    41 #define RAW_ACCEL_MAG_DATA_SIZE 12    42 #define FXOS8700_STREAM_DATA_SIZE 17    45 #define APPLICATION_NAME "FXOS8700 6-axis (Accel, Mag) Demo"    47 #define APPLICATION_VERSION "2.5"   148     uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, 
size_t *hostMsgSize, 
size_t respBufferSize)
   150     bool success = 
false;
   165         if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
   174         hostResponse[*hostMsgSize] = appNameLen;
   177         memcpy(hostResponse + *hostMsgSize, 
embAppName, appNameLen);
   178         *hostMsgSize += appNameLen;
   180         hostResponse[*hostMsgSize] = boardNameLen;
   183         memcpy(hostResponse + *hostMsgSize, 
boardString, boardNameLen);
   184         *hostMsgSize += boardNameLen;
   186         hostResponse[*hostMsgSize] = shieldNameLen;
   189         memcpy(hostResponse + *hostMsgSize, 
shieldString, shieldNameLen);
   190         *hostMsgSize += shieldNameLen;
   200         switch (hostCommand[0]) 
   262     if (ARM_DRIVER_OK != status)
   268     status = I2Cdrv->PowerControl(ARM_POWER_FULL);
   269     if (ARM_DRIVER_OK != status)
   275     status = I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   276     if (ARM_DRIVER_OK != status)
   283     if (ARM_DRIVER_OK != status)
   289     status = pUartDriver->PowerControl(ARM_POWER_FULL);
   290     if (ARM_DRIVER_OK != status)
   297     if (ARM_DRIVER_OK != status)
   353         if (ARM_DRIVER_OK != status)
   362         rawData.
accel[0] = ((int16_t)data[0] << 8) | data[1];
   363         rawData.
accel[0] /= 4;
   364         rawData.
accel[1] = ((int16_t)data[2] << 8) | data[3];
   365         rawData.
accel[1] /= 4;
   366         rawData.
accel[2] = ((int16_t)data[4] << 8) | data[5];
   367         rawData.
accel[2] /= 4;
   368         rawData.
mag[0] = ((int16_t)data[6] << 8) | data[7];
   369         rawData.
mag[1] = ((int16_t)data[8] << 8) | data[9];
   370         rawData.
mag[2] = ((int16_t)data[10] << 8) | data[11];
   376         if((regdata & 0x04) == 0x04)
   381         else if((regdata & 0x02) == 0x02)
 
int32_t FXOS8700_I2C_Initialize(fxos8700_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
 
#define FXOS8700_PL_CFG_DBCNTM_CLEAR_MODE
 
#define FXOS8700_A_FFMT_CFG_YEFE_RAISE_EVENT
 
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
 
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
 
This structure defines the Write command List. 
 
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
 
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_MASK
 
#define FXOS8700_CTRL_REG5_INT_CFG_DRDY_MASK
 
#define FXOS8700_CTRL_REG4_INT_EN_DRDY_EN
 
#define RAW_ACCEL_MAG_DATA_SIZE
 
#define FXOS8700_A_FFMT_CFG_XEFE_MASK
 
ARM_DRIVER_I2C * pCommDrv
 
char shieldString[ADS_MAX_STRING_LENGTH]
 
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
 
const registerwritelist_t fxos8700_Config_InterruptHybrid[]
 
#define FXOS8700_M_CTRL_REG1_M_OS_MASK
 
The host_io_uart.h file contains the Host Protocol interface definitions and configuration. 
 
#define FXOS8700_M_CTRL_REG1_M_HMS_MASK
 
const registerreadlist_t FXOS8700_ACCEL_READ[]
 
#define FXOS8700_WHO_AM_I_PROD_VALUE
 
#define FXOS8700_CTRL_REG1_DR_MASK
 
#define HOST_PRO_CMD_W_CFG_TAG
 
Access structure of the GPIO Driver. 
 
#define FXOS8700_M_CTRL_REG1_M_HMS_HYBRID_MODE
 
GENERIC_DRIVER_GPIO * pGpioDriver
 
#define FXOS8700_A_FFMT_CFG_OAE_FREEFALL
 
#define __END_WRITE_DATA__
 
#define FXOS8700_M_CTRL_REG2_M_AUTOINC_HYBRID_MODE
 
void(* clr_pin)(pinID_t aPinId)
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
#define HOST_S_SIGNAL_EVENT
 
#define FXOS8700_A_FFMT_CFG_OAE_MASK
 
#define FXOS8700_CTRL_REG3_PP_OD_MASK
 
#define I2C_S_SIGNAL_EVENT
 
This defines the sensor specific information for I2C. 
 
int32_t FXOS8700_I2C_Configure(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
 
char embAppName[ADS_MAX_STRING_LENGTH]
 
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
 
#define BOARD_DEBUG_UART_BAUDRATE
 
int32_t FXOS8700_I2C_ReadData(fxos8700_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
#define FXOS8700_CTRL_REG4_INT_EN_DRDY_MASK
 
#define BOARD_BootClockRUN
 
#define FXOS8700_PL_CFG_DBCNTM_MASK
 
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
#define FXOS8700_M_CTRL_REG1_M_ACAL_EN
 
#define FXOS8700_A_FFMT_CFG_ZEFE_RAISE_EVENT
 
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
 
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick. 
 
#define FXOS8700_M_CTRL_REG1_M_ACAL_MASK
 
This structure defines the fxos8700 raw data buffer. 
 
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time. 
 
uint8_t data[FXLS8962_DATA_SIZE]
 
char boardString[ADS_MAX_STRING_LENGTH]
 
volatile bool bStreamingEnabled
 
#define FXOS8700_CTRL_REG5_INT_CFG_DRDY_INT2
 
#define __END_READ_DATA__
 
#define HOST_PRO_INT_DEV_TAG
 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
 
#define FXOS8700_XYZ_DATA_CFG_FS_MASK
 
#define FXOS8700_CTRL_REG1_DR_HYBRID_100_HZ
 
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
 
fxos8700_accelmagdata_t rawData
 
const registerreadlist_t cFXOS8700_pl_status[]
 
#define FXOS8700_CTRL_REG2_MODS_HIGH_RES
 
#define FXOS8700_XYZ_DATA_CFG_FS_2G_0P244
 
const registerreadlist_t cFXOS8700_ffmt_src[]
 
#define FXOS8700_A_VECM_THS_MSB_A_VBECM_THS_MASK
 
volatile bool bFxos8700DataReady
 
#define FXOS8700_PL_BF_ZCOMP_ZLOCK_MASK
 
void(* toggle_pin)(pinID_t aPinId)
 
#define ADS_MAX_STRING_LENGTH
 
The fxos8700_drv.h file describes the fxos8700 driver interface and structures. 
 
int main(void)
Main function. 
 
#define FXOS8700_PL_BF_ZCOMP_BKFR_MASK
 
#define FXOS8700_CTRL_REG2_MODS_MASK
 
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
 
#define STREAMING_HEADER_LEN
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
volatile bool bFxos8700Ready
 
This structure defines the Read command List. 
 
#define FXOS8700_STREAM_DATA_SIZE
 
gpioHandleKSDK_t GREEN_LED
 
#define I2C_S_DEVICE_INDEX
 
#define FXOS8700_CTRL_REG3_PP_OD_PUSH_PULL
 
void FXOS8700_I2C_SetIdleTask(fxos8700_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
#define FXOS8700_CTRL_REG3_IPOL_MASK
 
#define FXOS8700_A_FFMT_THS_THS_MASK
 
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6). 
 
#define FXOS8700_PL_CFG_PL_EN_MASK
 
#define FXOS8700_A_VECM_THS_MSB_A_VBECM_DBCNTM_MASK
 
void fxos8700_isr_callback(void *pUserData)
 
#define FXOS8700_I2C_ADDR
 
#define FXOS8700_A_FFMT_CFG_YEFE_MASK
 
#define FXOS8700_A_FFMT_CFG_ZEFE_MASK
 
registerDeviceInfo_t deviceInfo
 
#define FXOS8700_CTRL_REG3_IPOL_ACTIVE_HIGH
 
#define FXOS8700_PL_CFG_PL_EN_ENABLE
 
const registerreadlist_t cFXOS8700_int_src[]
 
#define FXOS8700_M_CTRL_REG1_M_OS_OSR0
 
#define FXOS8700_A_FFMT_CFG_XEFE_RAISE_EVENT