This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

ccm_clockout

Overview

The ccm_clockout driver example shows how to output the internal clock signal. In this driver example, users can choose the clock signal to be outputted, and the divider of the output clock signal. By probing the output pin, users can observe the selected internal clock signal. Please note that different targets may have different default clock configurations, so the frequency of the same clock root may be different in different targets even though the dividers are set as the same value.

Supported Boards