This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

mmdvsq

Overview

The MMDVSQ Example project is a demonstration program that uses the KSDK software to Calculation square root and Quotient

MMDVSQ Peripheral Driver Example

Start MMDVSQ Example Calculation square root, please enter radicand Square root of 9 is 3 Calculation division to get remainder and quotient Enter dividend and divisor Remainder of 10 and 5 is 0 Quotient of 10 and 5 is 2

Supported Boards