This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

syspm

Overview

The SYSPM project is a simple demonstration program of the SDK SYSPM driver.

The System Performance Monitor (SYSPM) is a memory mapped peripheral that enables the user to monitor system and/or CPU events. This demo project obtains the event count value through the system performance monitor, and prints three values.

Supported Boards