This is the documentation for the latest (main) development branch of
mcuxpresso sdk. If you are looking for the documentation of previous releases, use
the drop-down menu on the left and select the desired version.
kbi
Overview
The KBI Example project is a demonstration program that uses the KSDK software to use
keyboard interrupt.
The example uses one KBI pin to generate a raising edge interrupt to show the example.