This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

xbar

Overview

The Xbar project is a simple demonstration program of the SDK Xbar driver.The intended application of this module is to provide a flexible crossbar switch function that allows any input to be connected to any output under user control.It sets up the Xbar hardware block to trigger a periodic interrupt after every 1 second. When the Xbar interrupt is triggered a message a printed on the UART terminal.

Supported Boards