This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

wdog01

Overview

The WDOG Example project is to demonstrate usage of the KSDK wdog driver. In this example,implemented to test the wdog. Please notice that because WDOG control registers are write-once only. And for the field WDT, once software performs a write “1” operation to this bit, it can not be reset/cleared until the next POR, this bit does not get reset/ cleared due to any system reset. So the WDOG_Init function can be called only once after power reset when WDT set, and the WDOG_Disable function can be called only once after reset.

Supported Boards