This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

epit

Overview

The EPIT project is a simple demonstration program of the SDK EPIT driver. It sets up the EPIT hardware block to trigger a periodic interrupt after every 1 second. When the EPIT interrupt is triggered a message a printed on the UART terminal.