This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

opamp_basic

Overview

This project shows how to use the OPAMP driver. In this example, the OPAMP works in the internal gain mode, the positive terminal of the OPAMP is connected to the external input source, and the OPAMP output comes from 2X of the external input voltage. When the input voltage changes, the OPAMP output changes accordingly.

Supported Boards