This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

sysctr

Overview

The sysctr example shows the usage of System Counter driver in application. The System Counter provides a shared time base to multiple processors. It is intended for applications where the counter is always powered on, and supports multiple unrelated clocks.

In this example, System Counter is clocked by 24MHz base clock. System Counter count value will be printed at 3 second and 5 second.

Supported Boards