This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

itrc_1

Overview

The ITRC Example project is a demonstration program that uses the MCUX SDK software to set up Intrusion and Tamper Response Controller. Then tests the expected behaviour.

Running the demo

When the demo runs successfully, the terminal displays similar information like the following:


ITRC Peripheral Driver Example

Pass: No Event/Action triggered after Init

Enable ITRC IRQ Action response to SW Event 0

Trigger SW Event 0

ITRC IRQ Reached!
ITRC STATUS0:
Software event 0 occurred!
ITRC triggered ITRC_IRQ output!

Clear ITRC IRQ and SW Event 0 STATUS

Disable ITRC IRQ Action response to SW Event 0

Trigger SW Event 0

Pass: No Action triggered after disabling

End of example

Supported Boards