This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dsc_cop

Overview

The COP Example project is to demonstrate usage of the cop driver.In this example, after 5 times of refreshing in interrupt routine, interrupt will be disabled, thus the COP is not serviced, then a timeout reset is generated. Please notice that Write Protect bit in CTRL register are write-once only, it can be cleared only by resetting COP module. All COP registers are read-only when Write Protect bit set.

Supported Boards