This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

crc

Overview

The CRC Example project is a demonstration program that uses the KSDK software to generate checksums for an ASCII string. Several CRC protocols are implemented using the CRC driver API.

Running the demo

Example output on terminal:

CRC Peripheral Driver Example

Test string: 123456789 CRC-16 CCIT FALSE: 0x29b1 CRC-16 MAXIM: 0x44c2 CRC-16 KERMIT: 0x2189 CRC-32: 0xcbf43926 CRC-32 POSIX: 0x765e7680

Supported Boards