This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

irtc

Overview

The IRTC project is a simple demonstration program of the SDK IRTC driver. This example is a low power module that provides time keeping and calendaring functions and additionally provides protection against tampering, protection against spurious memory/register updates and battery operation.

Supported Boards