This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpc_cic_irb

Overview

The IRB Example project is a demonstration program that uses the Infra-Red Blaster (IRB) peripheral software. It performs a sequence of sending packets.

Running the demo

The log below shows example output of the IRB driver demo in the terminal window:

IR Blaster example
Sending 10 RC-5 packets...
Packet 1
Packet 2
Packet 3
Packet 4
Packet 5
Packet 6
Packet 7
Packet 8
Packet 9
Packet 10
Bye.