This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

sha

Overview

The SHA Example project is a demonstration program that uses the KSDK software to generate SHA checksums.

Running the demo

The log below shows example output of the SHA driver demo in the terminal window:

SHA Peripheral Driver Example

Calculating SHA-256 digest.
Input: Hello SHA-256 world. Hello SHA-256 world. Hello SHA-256 world. Hello SHA-256 world.
Output: E68675E9ACFF8B57E386312E85371E6410BECCE2A249001955C45C98CBE5373E

Supported Boards