This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

vref_example

Overview

The vref example shows how to use the vref driver.

In this example, the adc16 module is initialized and used to measure the VREF output voltage. So, it cannot use internal VREF as the reference voltage.

Then, user should configure the VREF output pin as the ADC16’s sample input. When running the project, it will firstly measure the VREF output voltage within the default (factory) trim value. Then, it will measure the VREF output voltage under different trim values.

Supported Boards