This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

gdet

Overview

Running the demo

When the demo runs successfully, the terminal displays similar information like the following:


GDET Peripheral Driver Example

GDET Init
GDET Enable
GDET Isolate
* Now VDD voltage can be adjusted *
GDET Change voltage mode
GDET Isolation off

End of example

## Supported Boards
- [FRDM-MCXN947](../../_boards/frdmmcxn947/driver_examples/gdet/example_board_readme.md)
- [MCX-N5XX-EVK](../../_boards/mcxn5xxevk/driver_examples/gdet/example_board_readme.md)
- [MCX-N9XX-EVK](../../_boards/mcxn9xxevk/driver_examples/gdet/example_board_readme.md)
- [MIMXRT700-EVK](../../_boards/mimxrt700evk/driver_examples/gdet/example_board_readme.md)