This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

tdet

Overview

The TDET Example project is a demonstration program that uses the MCUX SDK software to set up Digital Tamper (TDET) peripherial. Then tests the expected behaviour.

Running the demo

When the demo runs successfully, the terminal displays similar information like the following:


TDET Peripheral Driver Example

Tampering detected Tamper Detect Flag is set

Passive tamper example
No tampering detected on PIN0

Active tamper example
No tampering detected on active tamper

End of example

Supported Boards