This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

glikey

Overview

The GLIKEY Example project is a demonstration program that uses the MCUX SDK software to set up GLIKEY IP peripherial.

Running the demo

When the demo runs successfully, the terminal displays similar information like the following:


GLIKEY Peripheral Driver Example

*Success* GLIKEY is not locked

*Success* GLIKEY Sync Reset done

*Success* GLIKEY Start enable done

*Success* GLIKEY Continue enable Step 1 pass

*Success* GLIKEY Continue enable Step 2 pass

*Success* GLIKEY Continue enable Step 3 pass

*Success* GLIKEY Continue enable  Step 4 pass

*Success* GLIKEY Continue enable  Step 5 pass

*Success* GLIKEY Continue enable  Step 6 pass

*Success* GLIKEY Continue enable  Step 7 pass

*Success* GLIKEY Continue enable Step Enable pass

SUCCESS: Register on index 2 can be now written!

*Success* GLIKEY End of operation done

End of example

Supported Boards