This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

utick_example

Overview

The utick project is a simple demonstration program of the SDK utick driver. It sets up the utick hardware block to trigger a periodic interrupt after every 1 second. When the utick interrupt is triggered a message a printed on the UART terminal.

Supported Boards