This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

rtwdog

Overview

The RTWDOG Example project is to demonstrate usage of the KSDK rtwdog driver. In this example, fast testing is first implemented to test the rtwdog. After this, refreshing the watchdog in None-window mode and window mode is executed. Note rtwdog is disabled in SystemInit function which means rtwdog is disabled after chip emerges from reset.

Supported Boards