This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lmemc

Overview

The local memory controller cache example shows how to use local memory cache driver.

In this example, the sdram memory will be used to show the example. The sdram memory is both accessible for cpu and EDMA. For the memory data alignment, cache driver should be used rightly. The code cache driver and system cache driver can be used when the relevant cache mode is enabled. In code cache enabled case, the code cache enabled memory mapped in sdram is write though/non-cacheable mode. so the sdram memory invalidate should be done before cpu read the memory. In system cache enabled case, when the sdram memory is write-back mode, the memory invalidate should be done before cpu read the memory and the memory push should be done before EDMA access the memory.