This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

acmp_round_robin

Overview

The ACMP Round-Robin project is a simple demonstration program that uses the SDK software. User must set the round-robin mode trigger in specific board properly according to the board resource before running the example. When the example running, it sets positive port as fixed channel and internal DAC output as comparison reference in positive port and sets the channels input by user as round-robin checker channel. The example will enter stop mode and wait user to change the voltage of round-robin checker channel. It will exit stop mode after the voltage of round-robin checker channel changed by user.

Running the demo

When the demo runs successfully, following information can be seen on the OpenSDA terminal:

Example to demonstrate low power wakeup by round robin comparison!
In order to wakeup the MCU, please change the analog input voltage to be different from original pre-state setting.

Press S for enter: Stop Mode

The system entered into stop mode.

The system exited from stop mode!

Supported Boards