This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

adc_5v12b_ll18_015_interrupt

Overview

The adc_interrupt example shows how to use interrupt with adc driver.

In this example, user should indicate a channel to provide a voltage signal (can be controlled by user) as the adc’s sample input. When running the project, typing any key into debug console would trigger the conversion. ADC interrupt would be asserted once the conversion is completed. In ADC ISR, the conversion completed flag would be cleared by reading the conversion result value. Also, the conversion result value is stored, and the ISR counter is increased. These information would be printed when the execution return to the main loop.

The point is that the adc interrupt configuration is set when configuring the adc’s conversion channel. When in software trigger mode, the conversion would be launched by the operation of configuring channel, just like writing a conversion command. So if user wants to generate the interrupt every time the conversion is completed, the channel’s configuration with enabling interrupt setting would be used for each conversion.

Supported Boards